web
You’re offline. This is a read only version of the page.
close
Template "Setup IS VAR Menu" not found.

Rockwell Automation Reports First Quarter 2022 Results

The following information was recently announced in the Rockwell Automation Q1 FY22 press release:

  • Record quarterly orders of $2.5 billion, up over 40% year over year
  • Reported sales up 18.7% year over year; organic sales up 16.8%
  • Reaffirms fiscal 2022 reported sales growth guidance of 16% - 19%; organic sales growth of 14% - 17%

Click here to see the full press release.